Digi-Key Corporation Announces Stock on the ABPSM-ULN-A Power Supply Module from Abracon

THIEF RIVER FALLS, Minnesota, USA - June 18, 2010

Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced it has stock on the ABPSM-ULN-A ultra low noise power supply module from Abracon Corporation.

  • ABPSM-ULN-A (Digi-Key #535-10307-ND) Power Supply Module, 4-channel, Low Noise

This new product is now available for purchase on Digi-Key's global websites and will be featured in future print and online catalogs.

The ABPSM-ULN-A module provides an ultra low noise, power supply source (25 nV/√Hz maximum & 1 kHz) with four regulated DC outputs. Offering 1.8 V, 2.5 V, 3.3 V and 5.0 V DC bias ports, this module is uniquely positioned to replace multiple, low noise, linear power supplies, which are typically needed to bias noise sensitive circuitry.

The ABPSM-ULN-A is designed to utilize a universal low noise AC adapter, enabling worldwide functionality, accepting 100 VAC to 240 VAC and 50 Hz and 60 Hz cycles. Coupled with state-of-the-art low noise regulation, this power supply module (PSM) provides an optimal setup to conduct noise sensitive measurements of system critical circuitry, such as phase noise, jitter, spectral purity, and signal to noise ratio.

Features of the ABPSM-ULN-A include 100 VAC to 240 VAC AC adapter input voltage; 50 Hz and 60 Hz cycles; four DC output ports – 1.8 V, 2.5 V, 3.3 V and 5.0 V; current sourcing capability per port 200 mA max. (each port); and ultra low noise characteristics to include < 0.30 µVrms over 0.1 Hz to 1 kHz bandwidth and a typical Noise Density & 1 kHz offset per the following profile:

  • 4 nV√Hz for 1.80 V DC Output; 5 nV√Hz for 2.50 V DC Output; 7 nV√Hz for 3.30 V & 15 nV√Hz for 5.00 V DC Output

About Digi-Key Corporation

Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.

About Abracon Corporation

Abracon Corporation, founded in 1992, is a privately held California corporation and is a worldwide leading supplier of Frequency Control and Magnetic components. Abracon (www.abracon.com) offers a wide selection of Crystal & MEMS based oscillators, quartz crystals, ceramic resonators, filters, SAW devices, inductors, ferrite beads, chokes. The company is ISO9001:2008 certified and has manufacturing facilities certified to ISO9001:2000 & TS16949 standards. For global customer support, Abracon has direct sales and engineering offices located in California, China, Taiwan, Singapore, and Germany. In addition, Abracon products are marketed worldwide through independently owned contracted representatives and authorized distributors.

Editorial Contact for Digi-Key Corporation
Erica Hanson
publicrelations@digikey.com