In the large gray bubble toward the top of the slide are technologies that are being developed or that have recently been introduced to the market. In the 5xx-6xx new generation family, are the F541x and the F543x; basically everything else in this large gray bubble is based on this new architecture. This includes the USB devices now on the market, which are the F550x, F551x, and F552x families. Another group of devices is our native sub-1V family that operates down to 0.9V without a regulator. And our FRAM-memory based devices with unique benefits such as fast write times and lower power consumption are already sampling. TI is also involved with integrating RF functionality, such as the CC430 devices. Finally, also in development are MSP430 devices that will feature more memory and capability, enabling higher functionality such as hosting connectivity stacks or RTOS capabilities.